This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3101: 音频调试无声音输出

Part Number: TLV320AIC3101
Other Parts Discussed in Thread: TLV320AIC31

最近在海思SS528平台上调试TLV320AIC3101的驱动,硬件做了一路MIC输入、一路LINE IN 输入和一路LINE OUT,原理图如下:

调试了好久,一直没有声音输出,我的寄存器配置:

void soft_reset(unsigned int chip_num)
{
    // soft reset
    tlv320aic31_write(IIC_device_addr[chip_num], 1,0x80);
    msleep(10);

    /*CLKDIV_IN uses MCLK*/
    tlv320aic31_write(IIC_device_addr[chip_num], 102, 0x32);

#if 1
    /*PLL disable and select Q value*/
    tlv320aic31_write(IIC_device_addr[chip_num], 3, 0x10);
#else
    // PLL enable
    tlv320aic31_write(IIC_device_addr[chip_num], 3, 0x81);/* P=1 Q=16*/
    tlv320aic31_write(IIC_device_addr[chip_num], 4, 0x20);/* J=8 */
    tlv320aic31_write(IIC_device_addr[chip_num], 5, 0x00);
    tlv320aic31_write(IIC_device_addr[chip_num], 6, 0x00);
#endif

    // left and right DAC open
    tlv320aic31_write(IIC_device_addr[chip_num], 7,  0x0a);/* 48 kHz */

    // sample
    tlv320aic31_write(IIC_device_addr[chip_num], 2, 0xaa);/* FS = FSref/6 */

    // ctrl mode
    tlv320aic31_write(IIC_device_addr[chip_num], 8,  0x00);/* slave mode */

    // Audio Serial Data Interface Control
    tlv320aic31_write(IIC_device_addr[chip_num], 9,  0x07);/* I2S mode,16bit */

    // Data offset = 0 bit clocks
    tlv320aic31_write(IIC_device_addr[chip_num], 10, 0x00);

    // Audio Codec Digital Filter Control Register
    tlv320aic31_write(IIC_device_addr[chip_num], 12, 0x50);
    tlv320aic31_write(IIC_device_addr[chip_num], 14, 0x00);

    // The ADC PGA is not muted.
    tlv320aic31_write(IIC_device_addr[chip_num], 15, 0x00);
    tlv320aic31_write(IIC_device_addr[chip_num], 16, 0x00);

    // LINE2L connected to the left ADC PGA
    tlv320aic31_write(IIC_device_addr[chip_num], 17,  0x0f);
    // LINE2R connected to the right ADC PGA
    tlv320aic31_write(IIC_device_addr[chip_num], 18,  0xf0);

    // LINE1LP is configured in single-ended mode
    // LINE1L connected to the left-ADC PGA
    // Left-ADC channel is powered up
    tlv320aic31_write(IIC_device_addr[chip_num], 19,  0x04);

    // LINE1RP is configured in single-ended mode
    tlv320aic31_write(IIC_device_addr[chip_num], 21,  0xC0);

    // LINE1RP is configured in single-ended mode
    // LINE1R connected to the right-ADC PGA
    // Right-ADC channel is powered up
    tlv320aic31_write(IIC_device_addr[chip_num], 22,  0x04);

    // LINE1LP is configured in single-ended mode
    tlv320aic31_write(IIC_device_addr[chip_num], 24,  0xC0);

    // Left DAC is powered up
    // Right DAC is powered up
    // HPLCOM is configured as independent single-ended output
    tlv320aic31_write(IIC_device_addr[chip_num], 37, 0xe0);

    // HPRCOM is configured as independent single-ended output
    tlv320aic31_write(IIC_device_addr[chip_num], 38, 0x10);

    // Left-DAC output selects DAC_L1 path,
    // Right-DAC output selects DAC_R1 path
    tlv320aic31_write(IIC_device_addr[chip_num], 41, 0x00);

    // PGA_L is routed to HPLOUT
    tlv320aic31_write(IIC_device_addr[chip_num], 46, 0x80);
    // DAC_L1 is routed to HPLOUT
    tlv320aic31_write(IIC_device_addr[chip_num], 47, 0x80);
    // PGA_R is routed to HPLOUT
    tlv320aic31_write(IIC_device_addr[chip_num], 49, 0x00);
    // DAC_R1 is routed to HPLOUT
    tlv320aic31_write(IIC_device_addr[chip_num], 50, 0x00);
    // HPLOUT is not muted, HPLOUT is fully powered up
    tlv320aic31_write(IIC_device_addr[chip_num], 51, 0x0f);

    // PGA_L is routed to HPLCOM.
    tlv320aic31_write(IIC_device_addr[chip_num], 53, 0x00);
    // DAC_L1 is routed to HPLCOM
    tlv320aic31_write(IIC_device_addr[chip_num], 54, 0x80);
    // PGA_R is routed to HPLCOM
    tlv320aic31_write(IIC_device_addr[chip_num], 56, 0x00);
    // DAC_R1 is routed to HPLCOM
    tlv320aic31_write(IIC_device_addr[chip_num], 57, 0x00);
    // HPLCOM is not muted, HPLCOM is fully powered up
    tlv320aic31_write(IIC_device_addr[chip_num], 58, 0x0f);

    // PGA_L is routed to HPROUT
    tlv320aic31_write(IIC_device_addr[chip_num], 60, 0x80);
    // DAC_L1 is routed to HPROUT
    tlv320aic31_write(IIC_device_addr[chip_num], 61, 0x80);
    // PGA_R is routed to HPROUT
    tlv320aic31_write(IIC_device_addr[chip_num], 63, 0x00);
    // DAC_R1 is routed to HPROUT
    tlv320aic31_write(IIC_device_addr[chip_num], 64, 0x00);
    // HPROUT is not muted, HPROUT is fully powered up
    tlv320aic31_write(IIC_device_addr[chip_num], 65, 0x0f);

    // PGA_L is routed to HPRCOM
    tlv320aic31_write(IIC_device_addr[chip_num], 67, 0x00);
    // DAC_L1 is routed to HPRCOM
    tlv320aic31_write(IIC_device_addr[chip_num], 68, 0x80);
    // PGA_R is routed to HPRCOM
    tlv320aic31_write(IIC_device_addr[chip_num], 70, 0x00);
    // DAC_R1 is routed to HPRCOM
    tlv320aic31_write(IIC_device_addr[chip_num], 71, 0x00);
    // HPRCOM is not muted, HPRCOM is fully powered up
    tlv320aic31_write(IIC_device_addr[chip_num], 72, 0x0f);  

    // The left-DAC channel is not muted.
    tlv320aic31_write(IIC_device_addr[chip_num], 43, 0x80);

    // The right-DAC channel is not muted
    tlv320aic31_write(IIC_device_addr[chip_num], 44, 0x80);
}

不知道我的这个寄存器配置与我的硬件原理图是否匹配吗?

  • 您好,register 15和16 的left ADC和right ADC gain设置的是0dB,建议增大增益再看看。

    同样寄存器R43,R44 left和right DACvolume也建议将volume control 增大,不使用0dB。

    R51 HPLOUT的output level也建议调大。

  • 谢谢您的解答,现在line in接入音频信号,line out有声音输出了。但是MIC输入还是没有声音,请问是哪里问题呢?line in 和 MIC in能够同时存在吗?是不是配置了line in之后MIC in就不起作用了

  • 您好,这款codec的line in和mic in是复用引脚,您的意思是channel 1 做line in, channel 2作为mic in是吗?

  • 我的硬件电路line in和mic in是独立的接口:MIC2L/LINE2L/MICDET、MIC2R/LINE2R 引脚作为 line in,MIC1RP/LINE1RP、MIC1RM/LINE1RM 引脚作为mic in。现在line out 能听到line in的输入声音,不能听到mic in的声音,是不是需要配置哪些寄存器呢?

  • 您好,通过内部架构可以看出,这几个输入是通过内部的mixing进行处理的。

    在mix之前集成是运放,可以看如下框图,这个是左通道的,右通道类似架构,听不到mic的声音,应该是运放前的开关没有配置,开关闭合之后这几个输入才会进入mixer,然后到left ADC PGA。 

  • 我向 Page 0/Register 21 写入0xc0,Page 0/Register 22 写入0xc4,但是还是听不到mic的声音,是不是我理解错了呢?

  • Page 0/Register 21

    您好,这个寄存器是配置MIC1RP/LINE1RP到left ADC的路由。

    Page 0/Register 22

    这个寄存器是配置的MIC1RP/LINE1RP到right ADC的路由。

    这样就矛盾了吧。

    另外,上述配置的都是按照mic 差分模式输入的。

    如果是差分的话MIC1RP/LINE1RP、MIC1RM/LINE1RM是mic right chanel的两个差分信号。

    那么左通道的MIC1LM/LINE1LM和MIC1LP/LINE1LP 应该也要配置的。

    如果单端输入的话,那么只使用MIC1RP和MIC1LP作为左右通道的单端输入。

  • 您好,能否加我QQ进一步指导一下,有偿。QQ:317397151

  • 您好,您的问题我会再继续跟进和确认的。

    另外,我们目前的支持方式是以论坛的方式和您沟通的,没有其他方式并且也是无偿的哈。

  • 我的电路上TLV320AIC31的MICBIAS引脚接地了,会对MIC的MIC1RP/LINE1RP、MIC1RM/LINE1RM引脚输入信号有影响吗?

  • MICBIAS是输出引脚,是headphone偏置输出电压,偏置输出电压的值可通过Page 0/Register 25 去配置,比如输出2V或者2.5V。

    接GND是Page 0/Register 25 配置的micbias output power down了吗?

    建议将其配置为一定的输出电压 ,比如2.5V 验证下。