现在设计阶段,根据EVM板子,板子尺寸问题不使用差分输入,两路SE输入,2 BTL输出。在此使用条件下,M1/M2管脚是否全部连接到GND也是没问题。
我单端输入,差分模式输出,这样是不是调整不了我功放的输出功率?如果接4Ω的音箱,36V的工作条件下,输出功率是否还能达到140W/4Ω,或者80W/8欧姆
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
如果已确定是BTL输出,可以将M1和M2接地。
具体请参考下面的评估板配置。
不同负载的输出功率,请参考芯片数据手册“Figure 4”和“Figure 5”。
www.ti.com.cn/.../tpa3251.pdf