This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK05028: LMK05028应用

Part Number: LMK05028

大家好,有个问题需要请教一下,问题如下:

我们有个编码器输出为10khz~50khz的信号,此信号实际为周期性脉冲信号,抖动约1%,我们想通过PLL芯片进行固定倍频数锁定,输出0.3Mhz~1.5mhz时钟信号(25ppm),然后传输至相机,进行触发。

应用环境:PLL锁定后持续输出时间约3s,3s后输入时钟信号消失,PLL即失锁;然后等待约50ms重新建立输入时钟,需要在这段时间内重新将PLL LOCK起来,如此循环往复。

针对以上应用场景,lmk05028芯片是否适用呢?10khz~50khz的信号,抖动为1%,是否会发生无法锁定的情况呢?