This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: LMX2594

Part Number: LMX2594

I am 1st time using LMX2594. Input clock is 100MHz, Output required is 1000MHz, But i do not  get.

Help check the following parameters:

Doubler:X2

PreR:1

Multiplier:bypass

R:1

FPD:200MHz

N divide:50

Output MUX:VCO

PFD_DLY_SEL:3

RFoutA:10000MHz

Whether the above settings are correct