采样方案为AMC1304M05输出后接数字隔离器ISO7841(仅仅使用一个通道),实现两级隔离,晶振提供时钟信号,数字隔离器ISO7841后接比较器TLV3501,5V供电,这样让高电平更加接近5V,比较器输出接三阶RC滤波器,截止频率30k左右,得到滤波后电压,作用相当于使用数字CIC滤波器!
测试发现有的电路板会出现1k左右的低频纹波,在50mV一格下看的很清楚,不知道是如何产生的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采样方案为AMC1304M05输出后接数字隔离器ISO7841(仅仅使用一个通道),实现两级隔离,晶振提供时钟信号,数字隔离器ISO7841后接比较器TLV3501,5V供电,这样让高电平更加接近5V,比较器输出接三阶RC滤波器,截止频率30k左右,得到滤波后电压,作用相当于使用数字CIC滤波器!
测试发现有的电路板会出现1k左右的低频纹波,在50mV一格下看的很清楚,不知道是如何产生的?
由于客户需要双重绝缘,所以增加了一级数字隔离器。由于我要对Delta_Segma输出的比特流,也即10M频率的一定占空比的方波进行滤波求平均,而数字隔离器比较器是电平芯片,高电平距离5V存在至少200mV的压摆,所以增加一级高速比较器TLV3501,100MHz带宽,4.5ns的delay,输出压摆20mV,可以使得输出的高电平更加接近5V,因此增加了一级比较器,这样整个系统的器件就增加了!
而且为了降低噪声我给比较器的电源是REF5050,我也测试了地和5V,在示波器打偏置下,50mV格度,并未观察到该低频纹波。
比较器的参考电平是2.5V,使用5V电源经过两个20k电阻分压得到,在引脚并联高频去耦电容,效果不是很明显!
我有六块板子,有三块出现了这个问题,还有三块这个问题不明显!
看一下比较器输出的波形,调整时间轴看看有没有低频的信号,另原理图发一下,谢谢。