想请问我这种设计方法正确吗?其次整个电路是共用一个GND吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
1、不需要的模拟输入接AVDD,没问题;
2、31脚 RESV1 根据手册说明需要接地;
3、SRB1 和SRB2、BIASREF、Reserved管脚不使用悬空,没问题;
4、模拟电源 ±2.5V双电源供电,没问题,请注意下AGND和GND是否单点连接,因为上图没有显示连接;
5、24和25脚是参考电压,这里不能悬空,如果使用内部参考电压,VREFP需要通过电容接VREFN,VREFN接AVSS;
6、关于CLK ,37脚和52脚,请根据下面真值表配置:
7、关于数字接口电平是以DVDD电压为标准的,DVDD这里是3.3V,那么CLK、CLKSEL管脚都属于数字接口,请输入3.3V的电平标准;
那么CLK有源时钟5V就是不可以的;CLKSEL 电平2.5V也是不可以的;
8、 如果不使用daisy-chaining模式,请将 DAISYIN管脚直接 DGND
9、关于GPIO,请按照下面方式连接:
最后,是的,共用一个GND