This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3683EVM: LPF in the ADC3683EVM

Part Number: ADC3683EVM
Other Parts Discussed in Thread: ADC3683

In the ADC3683EVM diagram, as shown by the left figure, there is an LPF(0~30 MHz) before the ADC3683. However, the datasheet (the right figure) of ADC3683 shows that the 3-dB bandwidth of ADC3683 is 900MHz. Does the LPF affect the ADC's performance if a signal with frequency larger than 30 MHz (such as 500 MHz) is sent to the AD3683EVM?