This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS8327外部基准电压的问题

Other Parts Discussed in Thread: ADS8327, ADS8328

在用ADS8327采样时,由于其不能采集负信号,因此需在外部将电压抬高,同时需要提供给ADS8327一个External Voltage Reference作为输入信号的range。现在遇到的问题是,希望外部作为抬高的电压为输给8327电压的一半,同时又能保证两个电压信号的稳定,请问除了使用两个电源芯片之外有什么比较好的方法,能够实现这样的操作?

  • 您好,您可以参考此图,其中1VDC可以通过两个电阻分压得到,可以从基准端分压。

  • 我担心的是分压不够准确,比如我给的reference是5V,分压的结果可能只有2.48V,那么我的转换结果会比实际的小(因为我会把减去2.5V),这样就可能造成采样的不准确。像ADS8328双通道输入就可以把分压也进行采样,就能比较准确了。但是ADS8327只有单通道输入,所以我不知道该如何保证采样的准确。

  • 分压的精确性您可以通过选择精密电阻解决,你可以选择千分之一精度或者更好的电阻,或者你可以挑选出匹配的电阻进行焊接,分压电阻阻值可以稍微小点,例如2k,防止运放偏置电流带来误差。