This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS52J91: ADS52J91和ADS52J90是否pin对pin,ADS52J91和能否直接替代ADS52J90?

Part Number: ADS52J91
Other Parts Discussed in Thread: ADS52J90,

ADS52J91和ADS52J90是否pin对pin,ADS52J91和能否直接替代ADS52J90?

  • 您好,

    ADS52J90和ADS52J91之间的主要区别是最大ADC转换率:

    – 100 MSPS in 10-Bit Mode for ADS52J90, 125 MSPS in 10-Bit Mode for ADS52J91
    – 80 MSPS in 12-Bit Mode for ADS52J90,  100 MSPS in 12-Bit Mode for ADS52J91
    – 65 MSPS in 14-Bit Mode for ADS52J90, 65 MSPS in 14-Bit Mode for ADS52J91

    功耗也有少许差别。

    关于是不是pin to pin,我再确认下,因为ADS52J91 datasheet未公开,内网正在维护打不开,我比对后再向您回复。

  • 它们封装是一样的,都是ZZE Package, 198-Pin NFBGA (15 mm × 9 mm)