This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3664EVM: ADC3664EVM

Part Number: ADC3664EVM

在芯片手册中看到如下图中的红框语句,请问ADC3664如果要输出DCLK的话,是不是就必须有DCLKIN输入,也就是说,ADC若没有接收到DCLKIN信号的话,也就不会输出DCLK信号。-----看法1

还是说:ADC3664始终会有DCLK信号输出,然后外部加入DCLKIN信号只是为了使得ADC能够控制DCLK输出的频率以便正确输出ADC转换数据。---------看法2

  • 您好,我认为看法1是正确的。DCLK是内部buffer的输出时钟,而DCLKIN作为buffer的参考时钟。

    所以如果DCLK有输出的话,需要有DCLKIN输入。

  • 我觉得是看法2正确。

    我的实验环境是:DCLKIN是由FPGA产生的并通过FMC路由给EVM,但是EVM的HD3SS3411IRWAT(即U2)器件中的sel引脚我是没有把它进行上拉的(即EVM板子默认是下拉),所以根据原理图来说,FPGA产生的信号DCLKIN_FPGA_P和DCLKIN_FPGA_N信号并不能通过这个U2器件,也就无法给ADC3664提供DCLKIN信号,但是我却能接回DCLK信号,你那边有实验环境可以测一下吗

  • FPGA产生的信号DCLKIN_FPGA_P和DCLKIN_FPGA_N信号并不能通过这个U2器件,也就无法给ADC3664提供DCLKIN信号,但是我却能接回DCLK信号

    您好,我再看下这个问题。

  • FPGA产生的信号DCLKIN_FPGA_P和DCLKIN_FPGA_N信号并不能通过这个U2器件,也就无法给ADC3664提供DCLKIN信号,但是我却能接回DCLK信号

    您好,HD3SS3411虽然没上拉,默认下拉的话,A port和C port导通,C port选的片上CDCE6214输出时钟作为DCLKIN的时钟输入。

    DCLKIN可以是外部时钟源输入(通过FPGA产生),也可以是片上onboard CDCE6214时钟发生器的输出,所以使用2:1开关HD3SS3411进行选择。