老师好:
我目前在使用TI公司的一个开发平台型号是TMDSHVMTRPFCKIT,平台上面有一块电平转换芯片TXB0106 将5v转成3.3v信号的,板子上是用来将电机的编码器反馈回来的5v的ABZ方波信号转成3.3v的方波信号的。我现在遇到的问题是芯片输入的ABZ(也就是电机反馈的方波信号)都是5V的,不知道在芯片的输出引脚的电压信号为什么只有A相是不对的 (A相输出电压的范围在1.8~2.2V) ;而B,Z相都是3V的方波信号。老师能帮我解答一下,问题可能出在哪里吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看 TXB0106 的手册, 各路功能没有什么区别, 怀疑外围电路造成的影响的可能性大
B、Z都正常,只有A不正常吗?输出1.8~2.2V可能是内部MOS损坏了,以前有没有输出短路过?换一个IC试试可不可以?
Airwill,你好:
A、B、Z三路的输入输出外围电路都是对称的,在输入芯片之前的各路电压波形我也确定过,都是5V左右的方波信号。如果说是芯片本身的问题,我换了一片也还是出现这样的情况。
如果三路信号是相同的话,应该和TXB106无关,或者将A路的信号换到其他没用的通道上试试,另外,如果你的信号一共3路的话,可以考虑同系列的4路的TXB0104,这样不用的通道只有一个。