Hi,
I am designing a data acquisition system base on ADS8881 to capture a sine wave signal from 0 ~100kHz(differential signal), my signal source is a little noisy, so I need to add an external low pass filter to achieve the best dynamic performance of ADS8881, my question is which type of low pass filter is the best chose for ADS8881 to achieve best SNR & THD in this application? I am thinking to use high order RLC low pass filter or MFB low pass filter, or is there other better solution? Is it possible to achieve the ADS8881 datasheet performance(100dB SNR, -115dB THD) in this application ? Please help!
Below is the FFT of my signal source.