This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131M08: 关于Global-chop和SYNC的使用

Part Number: ADS131M08

Hello!

1.在global-chop模式下,一次采样完成后,ADC会等待Global-chop delay时间之后,就自动开始下一次采样吗?其中“Sampling n”中的“n”是一个转换周期还是一个采样点?

2.如果将Global-chop delay [GC_DLY]设置足够长的时间,例如设置为最大的65536 tMOD,按照tMOD为 1/4.096M秒计算,GC_DLY最大可以延时0.016秒。

 这样如果在SYNC管脚上按照6400 Hz 产生一个触发信号,其周期为0.00015625秒,远小于GC_DLY的0.016秒。这样ADS131M08 是否就可以按照触发信号的6400 Hz进行采样?