This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3424: ADC3424 What is the output voltage of SPI communication

Part Number: ADC3424

What is the output voltage of SPI communication?

What is the output voltage when the input withstand voltage is 3.9V in the following table?