This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TIDA-01226参考原理图的疑问(2)

Other Parts Discussed in Thread: TIDA-01226

您好!

TIDA-01226参考原理图中,

在USB接口附近使用了一颗TLV70033DDC芯片(U47),目的是什么?

该芯片,可以将来自外部USB主机的5V电压(CY_VBUS)转换为3.3V电压(USB_LDO_3.3V),

由于回路中的FB21未安装,所以USB_LDO_3.3V并没有被使用,U47部分电路应该可以删除吧。

如果修改电路,不安装FB20,而安装FB21,那么即使整个信号板的电源并没有接入,

似乎U48桥接芯片也可由USB_LDO_3.3V供电,而正常启动。

不过即使这样,由于后端的FLASH并未上电,U48的启动意义又在哪里呢?

是为了预防,在信号板未上电的情况下,来自外部USB的5V电源电流,经由U48的P19脚,流向其他电路吗?