This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP9000X的相关应用问题

你好,,我们新谈了一个DMD的项目,客户的要求是
开发一个高速投影方案,DMD, 1920x1080,500Hz,6-8bit,cameralink 接口
我看了一下TI的资料
Up to 9523 Hz (1-Bit Binary Patterns)
– Up to 1031 Hz (8-Bit Gray Patterns PreLoaded With Illumination Modulation), External
Input Up to 360 Hz
按照1931HZ  8BIT换算500HZ  8bit应该的可以实现的,但我不太明白 8-Bit Gray Patterns PreLoaded With Illumination Modulation), External
Input Up to 360 Hz  这个的准确意思,是需要什么条件才能满足我的要求么或者有什么其它合适的物料可以推荐
谢谢!期待您的回复.