Other Parts Discussed in Thread: DLP4710, DLPA3005,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
@FLASH没有擦写完整:这个都是命令操作,在advanced操作读出来数据,然后按原来数据写之后系统就不能用了,必须重新烧录固件,请问这个是什么原因?
@slave没有写完整:这个还有其他的一些特征表象吗?
@系统初始化DMD没有识别:advanced可以读出来dmd的ID,系统也没有这个报错,为什么一读写flash,再读系统状态就会报flash Erase no Complete
@DLPA3005没有输出电压:这个1.1,1.8,3.3v电压都有输出。
1. 具体写了什么数据?投影显示正常吗?
2. 如果投影画面是全屏幕的,SLAVE DLPC3479就没有问题。
是否你的电路板上有FLASH而光机上的小板还有一组flash?
DLPC3479主从各一个FLASH。开机画面是完整吗?