在调试电路板的过程中发现,主控FPGA加载完程序后,DLPC410的init_active信号一直为高,表明初始化没完成,请问这是什么原因造成的。
主控FPGA在没有加载完成的时候,DLPC410的LED0具有闪烁灯光,LED1常亮,表明DLPC410应该是正常工作,但是我在chipscope里无法看到ini_actvie的状态,所以不确定LED1亮是不是一定是初始化完成了。
主控FPGA在加载后,经过约400ms将arstz信号设置为低,表示复位完成,其他信号,如NS_flip, comp_data都是设置为0,可以看到DLPC410 LED0等正常闪烁,但是LED1灯不亮。通过chipscope看到init_active信号为高,初始化未完成。主控输出的4路时钟信号均为200MHz差分。这个调试过程是没有加载DMD9500芯片的。所以想问下是什么原因造成初始化失败,难道一定要加载DMD芯片吗?
另外就是如果arstz信号如果没有设置成低,看到的情况是LED0和LED1都是常亮,按理说LED1常亮应该是初始化完成,但是我在chipscope上仍然看到init_active信号为高,所以LED1常亮表明初始化完成到底可靠不?