经实测不到10MHZ。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
通常以tpd的最大值(+10%)的倒数来估算传输速率,以SN74LVC245A为例,当Vcc=1.8V时,tpd(max)=12.2ns,那么可以计算1/(12.2+0.1)=81.3Mbps. 所以10M对于74LVC245A来说,是没有问题的
同样存在疑惑,根据Kailyn Chen 的回复,进一步搜索了下。
tpd的含义是平均传输延迟时间,这个值越小,开关速率越高。在有些手册中,可能没有这个具体值,可以通过这个公式计算得来:tpd=(tPHL+tPLH)/2;其中,tPHL是导通延迟时间,tPLH是截止延迟时间。
是的,不过我见到很多这类器件手册中还是给出了这个tpd的参数,事实上,信号最大的传输速率不仅仅和传输延迟是否匹配有关,还与输入信号的灵敏度,输出的上升沿和下降沿的边缘速率,同样在有时钟的情况下,也会影响到建立和保持时间,所以估算时,把传输延迟的最坏情况tpd(max)再+10%来计算的。
1除以(12.2+0.1)ns计算啊,换算成Mbps的话,大概就是81Mbps.