This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS160PR412: 使用场景、方案、方法确认以及仿真模型

Part Number: DS160PR412
Other Parts Discussed in Thread: DS160PR421, TMUXHS4412

在我们的设计中,FPGA支持EP模式和RC模式,我们选择DS160PR412和DS160PR421分别作为Demux/Mux,当作为RC模式时,SEL管脚为H时,选通为Port B,FPGA作为RC设备连接PCIe Slot。当作为EP设备时候,SEL管脚为L,选通Port A,FPGA作为EP设备连接到CPU,上电完成后,不做RC和EP的模式切换。

1)如上所述,框图如下,规格书中只提及了单个RC选通2个EP的方案,当前所提方案是否可行?

2)出于layout的考虑,我们将DS160PR412、DS160PR421的RX、TX接口对应所接的PCIe接口都做了PN极性翻转和ane线序翻转,前后保持一致,比如FPGA的TX3N连到了DS160PR412的RX0P,DS160PR412的TXA0P和TXB0P分别连到了CPU和PCIe Slot的RX3N,这样是否可行?

3)当前信号走线过长所以选择了DS160PR412和DS160PR421分别作为Demux/Mux,在我们测试验证后,可能会选择TMUXHS4412作为低成本方案,以上问题所列情况是否可以支持?

4)是否可以提供DS160PR412、DS160PR421用于SI仿真使用的信号仿真模型?