Other Parts Discussed in Thread: ALP
Dear TI:
DS90UB954通过同轴线跟953通讯,短的线缆15cm可以通讯成功,打开Camera Sensor,增加一根3m的延长线,953的I2C会通讯失败
请问需要排查供电电路还是哪里?多谢!~~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI:
DS90UB954通过同轴线跟953通讯,短的线缆15cm可以通讯成功,打开Camera Sensor,增加一根3m的延长线,953的I2C会通讯失败
请问需要排查供电电路还是哪里?多谢!~~
关于FPD_link信号质量,请问有什么测试放方法可以衡量?
使用ALP软件做阈值MAP 分析,参考这篇MAP 分析用户指南:
https://www.ti.com/lit/ug/snlu243/snlu243.pdf
另外,这篇是以953和960为例,如何做MAP分析的测试,请参考下:
DS90UB954通过同轴线跟953通讯,短的线缆15cm可以通讯成功,打开Camera Sensor,增加一根3m的延长线,953的I2C会通讯失败
3m的cable应该没问题的,您是使用的15cm+3m的延长线,还是直接使用3m的cable试的?
953 cable的距离应该是能到10m的,所以3m应该没问题。
Dear TI:
对比测试发现,跟主板S21的插损有关系。
请教一下使用954跟953通讯,对于线材的插损、阻抗要求是什么?有没有具体的指标?
还是说只能通过MAP眼图来实际测试?
您好,抱歉回复晚了,这是一篇关于FPD link cable的应用手册,可以参考下:
关于953和954搭配使用,最大的插值损耗在F=2.1Ghz时为20dB。总的插值损耗包含PCB以及cable的损耗应当要好于-10dB。
收到,感谢分享。再请教一个问题,953和954通讯过程中,用示波器监控LOCK、PASS引脚,打开摄像头时,预览过程中会概率性的拉低(10分钟左右)。请问正常吗?
概率性的拉低说明还是不稳定,这种不稳定要查下是哪里带来的不稳定,看下是不是cable的原因。