Other Parts Discussed in Thread: DS125DF410
DS100DF400SQ 是否支持2.5G 速率
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,关于您的这个问题,会尽快给您答复。
DS100DF400SQ 是否支持2.5G 速率
您好,我没有找到DS100DF400这个型号呢?题目中的DS100DF410每个channel能支持到 10.3125Gbps的速率。
您好,嗯这颗器件是定制芯片,所以在官网上查不到这个型号。
我看附件您提供的规格书里给出了每个通道的最大data rate也是10.3125Gbps。
我知道能到10.3125Gbps,需要确认是否支持2.5G 速率的,因为规格书有一句话说:For other data rates and data transmission protocols, other pin-compatible devices in the retimer family can be used
您好,我看了下它的数据手册, 可能是根据客户的实际需求进行定制的,它的主要data rate应用一个是10.3125Gbps,一个是1.25Gbps的应用,没有找到可以配置2.5Gbps的寄存器。所以不建议使用DF400进行2.5Gbps的应用。
您可以考虑使用DS125DF410。