This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: Auto-Negotiation Falied

Part Number: DP83867IS

Hi Ti experts,

My schematic is as follow。The PC cannot find the PHY when power on the circuit。

I do the following try:

1.Add the divider capacitor in XI pin as follows,the value of CD1 and CD2 is 27 pF.

2.Remove resistor R238 and R240;change the value of R235 to10 kΩ,and change the value of R236 to 2.49kΩ;let one pin of R236 connect to net ETHA_LED0 and another to  .

3.Change the RJ45 to the next circuit and connect  with by a capacitor of 4.7nF