由于中秋、国庆节假期,帖子审批以及工程师回复将会有所延迟,敬请谅解.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1042: CAN DC Bus Fault Protection Voltage: ±70 V

Part Number: ISO1042

规格书中的DC Bus Fault Protection Voltage: ±70 V,这具体的解释是什么?