This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO6762-Q1: 输入PWM信号,输出始终为高电平是什么原因?

Part Number: ISO6762-Q1
Other Parts Discussed in Thread: ISO7762-Q1,

VCC1用5V供电,VCC2用3.3V供电,INC接波形发生器,幅值为5V,频率1kHz,占空比50%,此时INC信号正常,OUTC始终为3.3V。请问可以判断数字隔离器已损坏吗?如果VCC1误接15V会导致数字隔离器损坏进而使输出一直为3.3V吗?请问有此类数字隔离器的应用电路实例吗?

  • 您好,

    很可能已经损坏,VCC最大耐压6V,超过6V会造成永久性损坏。

    如果VCC1误接15V会导致数字隔离器损坏进而使输出一直为3.3V吗?

    有可能使输出一直为3.3V。隔离件的输入接口如下截图所示,输入接口对VCC有二极管,如果输入高压击穿了二极管短路,那么内部输入可能与VCC短路,内部输入就一直是高电平,那么对应的输出就会是一直是高电平3.3V。

    请问有此类数字隔离器的应用电路实例吗?

    很抱歉,没有 ISO6762-Q1的参考设计,但是有类似器件 ISO7762-Q1的参考设计,下面链接设计中有使用 ISO7762-Q1:

    https://www.ti.com.cn/tool/cn/TIDA-020030