请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:INA240 您好!
下面是有关仿真的几个问题。
如何计算 INP 和 INN 的输入阻抗?
电流为10uA@5V、 85uA@10V、 105uA@20V
2.在数据表中、典型输入偏置为90uA。 当从分流电阻器到接地端有强制电流源时、如果电流限制在90uA 以下、INA240输出是否异常?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.