请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:OPA2376 主题中讨论的其他器件:OPA376、
您好!
当有两个不同的输入时、是否存在由于通道分离(0.5mV/V)引起的任何问题? 或关于如何限制疑虑的任何建议?
当 IC 关闭时、即使有耦合电容器、输入引脚(IN_A)也会影响音频信号吗?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.