大家好、
在实现"FSI_LOOP_POLLING_AM2434-EVM_r5fs"示例时、我收到以下错误。
我对 BOOT0-7的引导选择为"11011110"、对 BOOT8-15的引导选择为"01000000"。
我没有在任何 RAM 或 SD 卡中加载任何固件、只需使用 XDS110调试器实现上述示例。
请帮我解决问题、为什么我遇到上述错误。
等待您的反馈。
--
谢谢、此致、
Divyesh Patel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好、
在实现"FSI_LOOP_POLLING_AM2434-EVM_r5fs"示例时、我收到以下错误。
我对 BOOT0-7的引导选择为"11011110"、对 BOOT8-15的引导选择为"01000000"。
我没有在任何 RAM 或 SD 卡中加载任何固件、只需使用 XDS110调试器实现上述示例。
请帮我解决问题、为什么我遇到上述错误。
等待您的反馈。
--
谢谢、此致、
Divyesh Patel
Kowshik、您好!
感谢您的及时响应。
我已经访问了您提到的链接、但仍然无法进行调试。
现在处于调试阶段、但部分而言、我无法进入"fsi_loopback_solling_am243x_evm_r5ffss0"示例的环回状态。
请查找所附的映像和 linker.cmd 文件以供参考。
/* This is the stack that is used by code running within main()
* In case of NORTOS,
* - This means all the code outside of ISR uses this stack
* In case of FreeRTOS
* - This means all the code until vTaskStartScheduler() is called in main()
* uses this stack.
* - After vTaskStartScheduler() each task created in FreeRTOS has its own stack
*/
--stack_size=16384
/* This is the heap size for malloc() API in NORTOS and FreeRTOS
* This is also the heap used by pvPortMalloc in FreeRTOS
*/
--heap_size=32768
-e_vectors /* This is the entry of the application, _vector MUST be plabed starting address 0x0 */
/* This is the size of stack when R5 is in IRQ mode
* In NORTOS,
* - Here interrupt nesting is disabled as of now
* - This is the stack used by ISRs registered as type IRQ
* In FreeRTOS,
* - Here interrupt nesting is enabled
* - This is stack that is used initally when a IRQ is received
* - But then the mode is switched to SVC mode and SVC stack is used for all user ISR callbacks
* - Hence in FreeRTOS, IRQ stack size is less and SVC stack size is more
*/
__IRQ_STACK_SIZE = 256;
/* This is the size of stack when R5 is in IRQ mode
* - In both NORTOS and FreeRTOS nesting is disabled for FIQ
*/
__FIQ_STACK_SIZE = 256;
__SVC_STACK_SIZE = 4096; /* This is the size of stack when R5 is in SVC mode */
__ABORT_STACK_SIZE = 256; /* This is the size of stack when R5 is in ABORT mode */
__UNDEFINED_STACK_SIZE = 256; /* This is the size of stack when R5 is in UNDEF mode */
SECTIONS
{
/* This has the R5F entry point and vector table, this MUST be at 0x0 */
.vectors:{} palign(8) > R5F_VECS
/* This has the R5F boot code until MPU is enabled, this MUST be at a address < 0x80000000
* i.e this cannot be placed in DDR
*/
GROUP {
.text.hwi: palign(8)
.text.cache: palign(8)
.text.mpu: palign(8)
.text.boot: palign(8)
.text:abort: palign(8) /* this helps in loading symbols when using XIP mode */
} > MSRAM
/* This is rest of code. This can be placed in DDR if DDR is available and needed */
GROUP {
.text: {} palign(8) /* This is where code resides */
.rodata: {} palign(8) /* This is where const's go */
} > MSRAM
/* This is rest of initialized data. This can be placed in DDR if DDR is available and needed */
GROUP {
.data: {} palign(8) /* This is where initialized globals and static go */
} > MSRAM
/* This is rest of uninitialized data. This can be placed in DDR if DDR is available and needed */
GROUP {
.bss: {} palign(8) /* This is where uninitialized globals go */
RUN_START(__BSS_START)
RUN_END(__BSS_END)
.sysmem: {} palign(8) /* This is where the malloc heap goes */
.stack: {} palign(8) /* This is where the main() stack goes */
} > MSRAM
/* This is where the stacks for different R5F modes go */
GROUP {
.irqstack: {. = . + __IRQ_STACK_SIZE;} align(8)
RUN_START(__IRQ_STACK_START)
RUN_END(__IRQ_STACK_END)
.fiqstack: {. = . + __FIQ_STACK_SIZE;} align(8)
RUN_START(__FIQ_STACK_START)
RUN_END(__FIQ_STACK_END)
.svcstack: {. = . + __SVC_STACK_SIZE;} align(8)
RUN_START(__SVC_STACK_START)
RUN_END(__SVC_STACK_END)
.abortstack: {. = . + __ABORT_STACK_SIZE;} align(8)
RUN_START(__ABORT_STACK_START)
RUN_END(__ABORT_STACK_END)
.undefinedstack: {. = . + __UNDEFINED_STACK_SIZE;} align(8)
RUN_START(__UNDEFINED_STACK_START)
RUN_END(__UNDEFINED_STACK_END)
} > MSRAM
/* Sections needed for C++ projects */
GROUP {
.ARM.exidx: {} palign(8) /* Needed for C++ exception handling */
.init_array: {} palign(8) /* Contains function pointers called before main */
.fini_array: {} palign(8) /* Contains function pointers called after main */
} > MSRAM
/* General purpose user shared memory, used in some examples */
.bss.user_shared_mem (NOLOAD) : {} > USER_SHM_MEM
/* this is used when Debug log's to shared memory are enabled, else this is not used */
.bss.log_shared_mem (NOLOAD) : {} > LOG_SHM_MEM
/* this is used only when IPC RPMessage is enabled, else this is not used */
.bss.ipc_vring_mem (NOLOAD) : {} > RTOS_NORTOS_IPC_SHM_MEM
/* General purpose non cacheable memory, used in some examples */
.bss.nocache (NOLOAD) : {} > NON_CACHE_MEM
}
/*
NOTE: Below memory is reserved for DMSC usage
- During Boot till security handoff is complete
0x701E0000 - 0x701FFFFF (128KB)
- After "Security Handoff" is complete (i.e at run time)
0x701F4000 - 0x701FFFFF (48KB)
Security handoff is complete when this message is sent to the DMSC,
TISCI_MSG_SEC_HANDOVER
This should be sent once all cores are loaded and all application
specific firewall calls are setup.
*/
MEMORY
{
R5F_VECS : ORIGIN = 0x00000000 , LENGTH = 0x00000040
R5F_TCMA : ORIGIN = 0x00000040 , LENGTH = 0x00007FC0
R5F_TCMB0 : ORIGIN = 0x41010000 , LENGTH = 0x00008000
/* memory segment used to hold CPU specific non-cached data, MAKE to add a MPU entry to mark this as non-cached */
NON_CACHE_MEM : ORIGIN = 0x70060000 , LENGTH = 0x8000
/* when using multi-core application's i.e more than one R5F/M4F active, make sure
* this memory does not overlap with other R5F's
*/
MSRAM : ORIGIN = 0x70080000 , LENGTH = 0x40000
/* This section can be used to put XIP section of the application in flash, make sure this does not overlap with
* other CPUs. Also make sure to add a MPU entry for this section and mark it as cached and code executable
*/
FLASH : ORIGIN = 0x60100000 , LENGTH = 0x80000
/* shared memory segments */
/* On R5F,
* - make sure there is a MPU entry which maps below regions as non-cache
*/
USER_SHM_MEM : ORIGIN = 0x701D0000, LENGTH = 0x180
LOG_SHM_MEM : ORIGIN = 0x701D0000 + 0x180, LENGTH = 0x00004000 - 0x180
RTOS_NORTOS_IPC_SHM_MEM : ORIGIN = 0x701D4000, LENGTH = 0x0000C000
}
请帮我解决、我做了什么错。
--
谢谢、此致、
Divyesh Patel
您好、Divyesh、
您似乎正在将为 R5_0_0内核编译的代码加载到不起作用的 R50_1内核中。 您能否确保在正确的内核中加载?
谢谢
Kowshik、您好!
正确、首先我犯了错误、但后来在 R5_0_0内核中正确加载了它。
实际上、我有定制板、我认为我的问题与以下链接有关
我已经为 BOOT7-0选择了"01111011"、为 BOOT15-8选择了"00000010"、然后按照上面的链接执行操作。 在此过程中、我的代码卡在系统初始化函数中。
首先 、我想、我需要加载初始化脚本、然后我可以调试我的代码。
如果正确、您能否为我提供正确加载的正确顺序。
还请验证我的引导配置。
--
谢谢、此致、
Divyesh Patel
您好、Divyesh、
您共享的引导模式选项似乎与文档中的任何引导模式选项不匹配。 是否可以将其置于 No Boot 模式并运行 dmsc.js 脚本、该脚本会初始化内核、然后您是否可以尝试将代码加载到 R50_0?

谢谢
Kowshik、您好!
在该配置中、我无法连接处理器并收到以下错误。
我使用 XDS110 JTAG 进行调试。
--
谢谢、此致、
Divyesh Patel
您好、Divyesh、
在该模式下、您必须首先运行 SDK 中存在的 dmsc.js 脚本、以便首先初始化 SoC。 您无法直接连接到 R5内核。 请按照此命令和页面运行 dmsc 脚本。

AM243x MCU+ SDK:EVM 设置(TI.com)
此脚本运行后、您应该能够连接到 R5内核。
谢谢、
G Kowshik
Kowshik、您好!
在本例中、它尝试连接 M3。
--
谢谢、此致、
Divyesh Patel
您好、Divyesh、
您正在使用什么目标配置? 是的、dmsc 内核被认为连接到 M3内核、但它没有连接、因为您的目标连接可能错误。
您好、先生、
[引用 userid="525198" URL"~/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1191124/am2434-boot-setup-for-am2434/4493640 #4493640"]请使用什么目标配置?其 AM243x ALV
--
谢谢、此致、
Divyesh Patel
Kowshik、您好!
我收到另一个错误、请检查并帮助我解决。
请帮帮我。
--
谢谢、此致、
Divyesh Patel
您好、Divyesh、
我已将此主题分配给我们的 AM243x 专家、他将负责处理该主题。
谢谢、
G Kowshik
您好、Divyesh、
AM243x SoC 中存在硬件错误、JTAG 在上电后无法连接。 此问题已在下一个版本中修复。
解决方法是在为电路板加电后、您可能需要拔下并插入 JTAG。
此致、
Ming
您好、Ming、
感谢您的消息。
[引用 userid="15702" URL"~/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1191124/am2434-boot-setup-for-am2434/4494258 #4494258"]解决方法是在电路板上电后,您可能需要拔下并插入 JTAG。我也尝试过这种方法、但仍然遇到相同的问题
我是否犯了任何错误?
请指导我。
--
谢谢、此致、
Divyesh Patel
您好、Divyesh、
您是否正在使用"无引导"模式?

此致、
Ming
您好、Ming、
[引用 userid="15702" URL"~/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1191124/am2434-boot-setup-for-am2434/4495177 #4495177)]您是否使用了"不启动"模式? [/报价]是的、我使用相同的配置。
--
谢谢、此致、
Divyesh Patel
您好、Divyesh、
您能否尝试将目标配置中的"板或器件"从 AM2434_ALV 更改为 AM243x_GP_EVM?

您可以尝试使用最新的 MCU+ SDK 08.05.00。
此致、
Ming
您好、Ming、
是的、它现在工作了。
但是、为什么它不能与 AM243x_ALV 搭配使用? 是错误吗? 或者我遵循了一些错误的步骤?
--
谢谢、此致、
Divyesh Patel
您好、Divesh、
很高兴看到这对您有用。
我认为用于 ALV 与 EVM 的 GEL 文件是不同的。 ALV 文件中必须缺少一些与电路板相关的设置。
是否可以通过将此主题标记为"已解析"来关闭此主题?
谢谢!
Ming
您好、Ming、
非常感谢您的支持。
最后一个问题是、使用 EVM 配置是否合适?
或者我需要找到原因并设置为 ALV
—
谢谢、此致、
Divyesh Patel
您好、Divyesh、
您应该可以使用 AM243x_GP_EVM 而不是 AM243x_ALV、因为 AM243x_GP_EVM 是 AM243x_ALV 的超集。
此致、
Ming
您好、Ming、
非常感谢您的支持。
您的支持确实对我有帮助。
我要关闭此主题。
—
谢谢、此致、
Divyesh Patel