This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PCM5102A:每隔10秒发出一次声音

Guru**** 2507255 points
Other Parts Discussed in Thread: PCM5102A

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/audio-group/audio/f/audio-forum/1031847/pcm5102a-every-10-seconds-sound-stutters

器件型号:PCM5102A

我将 PCM5102A 与 QCC5144板结合使用。 I2S 配置如下所示(尝试在没有成功和明显差异的情况下更改):

CONST I2S_CONFIG_t DEVICE_I2S_CONFIG =

.master_mode = 1、
.data_format = 0、
bit_delay = 1、
.bits_per_sample_24、
.bclk_scaling = 48、
.MCLK_scaling = 0、
.ENABLE_PIO = PIN_INVALID
};

以下是具有此类缺陷的1kHz 正弦波(第6、第16和第26秒):

https://disk.yandex.ru/d/nCdE-lxIeViN2Q

如果配置了具有内置 DAC 的模拟输出、则一切都正常、因此我假设问题是 PCM5102A 配置。