请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TAS5711 TAS5711
电源电压12V;
输出功率:2x12w 最大400-500Hz 14W
2个喇叭、喇叭阻抗4 Ω
TAS5711产品在工作时、请使用热风机在高温下吹风以进行高温测试。 如果不是手动关闭,产品可以始终正常工作;但是,在关闭后,可以再次打开,并且只有在温度降低到50℃时才能正常工作。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.