主题中讨论的其他器件:SYSBIOS、 SIMPLELINK-CC13XX-CC26XX-SDK
我已按照电路板 TI-RTOS 基础知识的说明进行操作、从"hello"示例开始。 替换了"hello.c"的内容。 在"hello.cfg"中、删除了整个 ROM 块、启用了 BIOS 日志、并在结尾添加了3行带有日志记录设置
以下是"hello.cfg"文件内容:
/* * Copyright (c) 2015-2021, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* ================ Boot configuration ================ */ var Boot = xdc.useModule('ti.sysbios.family.arm.cc26xx.Boot'); /* * This module contains family specific Boot APIs and configuration settings. * See the SYS/BIOS API guide for more information. */ /* ================ Clock configuration ================ */ var Clock = xdc.useModule('ti.sysbios.knl.Clock'); /* * When using Power and calibrateRCOSC is set to true, this should be set to 10. * The timer used by the Clock module supports TickMode_DYNAMIC. This enables us * to set the tick period to 10 us without generating the overhead of additional * interrupts. * * Note: The calibrateRCOSC parameter is set within the Power configuration * structure in the "Board.c" file. */ Clock.tickPeriod = 10; /* ================ Defaults (module) configuration ================ */ var Defaults = xdc.useModule('xdc.runtime.Defaults'); /* * A flag to allow module names to be loaded on the target. Module name * strings are placed in the .const section for debugging purposes. * * Pick one: * - true (default) * Setting this parameter to true will include name strings in the .const * section so that Errors and Asserts are easier to debug. * - false * Setting this parameter to false will reduce footprint in the .const * section. As a result, Error and Assert messages will contain an * "unknown module" prefix instead of the actual module name. * * When using BIOS in ROM: * This option must be set to false. */ //Defaults.common$.namedModule = true; Defaults.common$.namedModule = false; /* ================ Error configuration ================ */ var Error = xdc.useModule('xdc.runtime.Error'); /* * This function is called to handle all raised errors, but unlike * Error.raiseHook, this function is responsible for completely handling the * error with an appropriately initialized Error_Block. * * Pick one: * - Error.policyDefault (default) * Calls Error.raiseHook with an initialized Error_Block structure and logs * the error using the module's logger. * - Error.policySpin * Simple alternative that traps on a while(1) loop for minimized target * footprint. * Using Error.policySpin, the Error.raiseHook will NOT called. */ //Error.policyFxn = Error.policyDefault; Error.policyFxn = Error.policySpin; /* * If Error.policyFxn is set to Error.policyDefault, this function is called * whenever an error is raised by the Error module. * * Pick one: * - Error.print (default) * Errors are formatted and output via System_printf() for easier * debugging. * - null * Errors are not formatted or logged. This option reduces code footprint. * - non-null function * Errors invoke custom user function. See the Error module documentation * for more details. */ //Error.raiseHook = Error.print; Error.raiseHook = null; //Error.raiseHook = "&myErrorFxn"; /* * If Error.policyFxn is set to Error.policyDefault, this option applies to the * maximum number of times the Error.raiseHook function can be recursively * invoked. This option limits the possibility of an infinite recursion that * could lead to a stack overflow. * The default value is 16. */ Error.maxDepth = 2; /* ================ Hwi configuration ================ */ var halHwi = xdc.useModule('ti.sysbios.hal.Hwi'); var m3Hwi = xdc.useModule('ti.sysbios.family.arm.m3.Hwi'); /* * Checks for Hwi (system) stack overruns while in the Idle loop. * * Pick one: * - true (default) * Checks the top word for system stack overflows during the idle loop and * raises an Error if one is detected. * - false * Disabling the runtime check improves runtime performance and yields a * reduced flash footprint. */ //halHwi.checkStackFlag = true; halHwi.checkStackFlag = false; /* * The following options alter the system's behavior when a hardware exception * is detected. * * Pick one: * - Hwi.enableException = true * This option causes the default m3Hwi.excHandlerFunc function to fully * decode an exception and dump the registers to the system console. * This option raises errors in the Error module and displays the * exception in ROV. * - Hwi.enableException = false * This option reduces code footprint by not decoding or printing the * exception to the system console. * It however still raises errors in the Error module and displays the * exception in ROV. * - Hwi.excHandlerFunc = null * This is the most aggressive option for code footprint savings; but it * can difficult to debug exceptions. It reduces flash footprint by * plugging in a default while(1) trap when exception occur. This option * does not raise an error with the Error module. */ //m3Hwi.enableException = true; //m3Hwi.enableException = false; m3Hwi.excHandlerFunc = null; /* * Enable hardware exception generation when dividing by zero. * * Pick one: * - 0 (default) * Disables hardware exceptions when dividing by zero * - 1 * Enables hardware exceptions when dividing by zero */ m3Hwi.nvicCCR.DIV_0_TRP = 0; //m3Hwi.nvicCCR.DIV_0_TRP = 1; /* * Enable hardware exception generation for invalid data alignment. * * Pick one: * - 0 (default) * Disables hardware exceptions for data alignment * - 1 * Enables hardware exceptions for data alignment */ m3Hwi.nvicCCR.UNALIGN_TRP = 0; //m3Hwi.nvicCCR.UNALIGN_TRP = 1; /* * Assign an address for the reset vector. * * Default is 0x0, which is the start of Flash. Ordinarily this setting should * not be changed. */ m3Hwi.resetVectorAddress = 0x0; /* * Assign an address for the vector table in RAM. * * The default is the start of RAM. This table is placed in RAM so interrupts * can be added at runtime. * * Note: To change, verify address in the device specific datasheets' * memory map. */ m3Hwi.vectorTableAddress = 0x20000000; /* ================ Idle configuration ================ */ var Idle = xdc.useModule('ti.sysbios.knl.Idle'); /* * The Idle module is used to specify a list of functions to be called when no * other tasks are running in the system. * * Functions added here will be run continuously within the idle task. * * Function signature: * Void func(Void); */ //Idle.addFunc("&myIdleFunc"); Idle.addFunc('&Power_idleFunc'); /* add the Power module's idle function */ /* ================ Kernel (SYS/BIOS) configuration ================ */ var BIOS = xdc.useModule('ti.sysbios.BIOS'); /* * Enable asserts in the BIOS library. * * Pick one: * - true (default) * Enables asserts for debugging purposes. * - false * Disables asserts for a reduced code footprint and better performance. * * When using BIOS in ROM: * This option must be set to false. */ //BIOS.assertsEnabled = true; BIOS.assertsEnabled = false; /* * Specify default CPU Frequency. */ BIOS.cpuFreq.lo = 48000000; /* * A flag to determine if xdc.runtime sources are to be included in a custom * built BIOS library. * * Pick one: * - false (default) * The pre-built xdc.runtime library is provided by the respective target * used to build the application. * - true * xdc.runtime library sources are to be included in the custom BIOS * library. This option yields the most efficient library in both code * footprint and runtime performance. */ //BIOS.includeXdcRuntime = false; BIOS.includeXdcRuntime = true; /* * The SYS/BIOS runtime is provided in the form of a library that is linked * with the application. Several forms of this library are provided with the * SYS/BIOS product. * * Pick one: * - BIOS.LibType_Custom * Custom built library that is highly optimized for code footprint and * runtime performance. * - BIOS.LibType_Debug * Custom built library that is non-optimized that can be used to * single-step through APIs with a debugger. * */ BIOS.libType = BIOS.LibType_Custom; //BIOS.libType = BIOS.LibType_Debug; /* * Runtime instance creation enable flag. * * Pick one: * - true (default) * Allows Mod_create() and Mod_delete() to be called at runtime which * requires a default heap for dynamic memory allocation. * - false * Reduces code footprint by disallowing Mod_create() and Mod_delete() to * be called at runtime. Object instances are constructed via * Mod_construct() and destructed via Mod_destruct(). * * When using BIOS in ROM: * This option must be set to true. */ BIOS.runtimeCreatesEnabled = true; //BIOS.runtimeCreatesEnabled = false; /* * Enable logs in the BIOS library. * * Pick one: * - true (default) * Enables logs for debugging purposes. * - false * Disables logging for reduced code footprint and improved runtime * performance. * * When using BIOS in ROM: * This option must be set to false. */ BIOS.logsEnabled = true; //BIOS.logsEnabled = false; /* ================ Memory configuration ================ */ var Memory = xdc.useModule('xdc.runtime.Memory'); /* * The Memory module itself simply provides a common interface for any * variety of system and application specific memory management policies * implemented by the IHeap modules(Ex. HeapMem, HeapBuf). */ /* * Use HeapMem primary heap instance to use linker-defined memory region */ var HeapMem = xdc.useModule('ti.sysbios.heaps.HeapMem'); HeapMem.primaryHeapBaseAddr = "&__primary_heap_start__"; HeapMem.primaryHeapEndAddr = "&__primary_heap_end__"; var heapMemParams = new HeapMem.Params(); heapMemParams.usePrimaryHeap = true; Program.global.heap0 = HeapMem.create(heapMemParams); Memory.defaultHeapInstance = Program.global.heap0; /* ================ Program configuration ================ */ /* * Program.stack must be set to 0 to allow the setting * of the system stack size to be determined in the example's * linker command file. */ Program.stack = 0; /* * Uncomment to enable Semihosting for GNU targets to print to the CCS console. * Please read the following TIRTOS Wiki page for more information on Semihosting: * processors.wiki.ti.com/.../TI-RTOS_Examples_SemiHosting */ if (Program.build.target.$name.match(/gnu/)) { //var SemiHost = xdc.useModule('ti.sysbios.rts.gnu.SemiHostSupport'); } /* ================ ROM configuration ================ */ /* * To use BIOS in flash, comment out the code block below. */ /* * CC13X1 and CC26X1 devices do not contain ROM; therefore, we do not include * the ROM module unless needed. */ /* ================ Semaphore configuration ================ */ var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore'); /* * Enables global support for Task priority pend queuing. * * Pick one: * - true (default) * This allows pending tasks to be serviced based on their task priority. * - false * Pending tasks are services based on first in, first out basis. * * When using BIOS in ROM: * This option must be set to false. */ //Semaphore.supportsPriority = true; Semaphore.supportsPriority = false; /* * Allows for the implicit posting of events through the semaphore, * disable for additional code saving. * * Pick one: * - true * This allows the Semaphore module to post semaphores and events * simultaneously. * - false (default) * Events must be explicitly posted to unblock tasks. * * When using BIOS in ROM: * This option must be set to false. */ //Semaphore.supportsEvents = true; Semaphore.supportsEvents = false; /* ================ Swi configuration ================ */ var Swi = xdc.useModule('ti.sysbios.knl.Swi'); /* * A software interrupt is an object that encapsulates a function to be * executed and a priority. Software interrupts are prioritized, preempt tasks * and are preempted by hardware interrupt service routines. * * This module is included to allow Swi's in a users' application. */ /* * Reduce the number of swi priorities from the default of 16. * Decreasing the number of swi priorities yields memory savings. */ Swi.numPriorities = 6; /* ================ System configuration ================ */ var System = xdc.useModule('xdc.runtime.System'); /* * The Abort handler is called when the system exits abnormally. * * Pick one: * - System.abortStd (default) * Call the ANSI C Standard 'abort()' to terminate the application. * - System.abortSpin * A lightweight abort function that loops indefinitely in a while(1) trap * function. * - A custom abort handler * A user-defined function. See the System module documentation for * details. */ //System.abortFxn = System.abortStd; System.abortFxn = System.abortSpin; //System.abortFxn = "&myAbortSystem"; /* * The Exit handler is called when the system exits normally. * * Pick one: * - System.exitStd (default) * Call the ANSI C Standard 'exit()' to terminate the application. * - System.exitSpin * A lightweight exit function that loops indefinitely in a while(1) trap * function. * - A custom exit function * A user-defined function. See the System module documentation for * details. */ //System.exitFxn = System.exitStd; System.exitFxn = System.exitSpin; //System.exitFxn = "&myExitSystem"; /* * Minimize exit handler array in the System module. The System module includes * an array of functions that are registered with System_atexit() which is * called by System_exit(). The default value is 8. */ System.maxAtexitHandlers = 2; /* * The System.SupportProxy defines a low-level implementation of System * functions such as System_printf(), System_flush(), etc. * * Pick one pair: * - SysMin * This module maintains an internal configurable circular buffer that * stores the output until System_flush() is called. * The size of the circular buffer is set via SysMin.bufSize. * - SysCallback * SysCallback allows for user-defined implementations for System APIs. * The SysCallback support proxy has a smaller code footprint and can be * used to supply custom System_printf services. * The default SysCallback functions point to stub functions. See the * SysCallback module's documentation. */ var SysMin = xdc.useModule('xdc.runtime.SysMin'); SysMin.bufSize = 512; System.SupportProxy = SysMin; //var SysCallback = xdc.useModule('xdc.runtime.SysCallback'); //System.SupportProxy = SysCallback; //SysCallback.abortFxn = "&myUserAbort"; //SysCallback.exitFxn = "&myUserExit"; //SysCallback.flushFxn = "&myUserFlush"; //SysCallback.putchFxn = "&myUserPutch"; //SysCallback.readyFxn = "&myUserReady"; /* ================ Task configuration ================ */ var Task = xdc.useModule('ti.sysbios.knl.Task'); /* * Check task stacks for overflow conditions. * * Pick one: * - true (default) * Enables runtime checks for task stack overflow conditions during * context switching ("from" and "to") * - false * Disables runtime checks for task stack overflow conditions. * * When using BIOS in ROM: * This option must be set to false. */ //Task.checkStackFlag = true; Task.checkStackFlag = false; /* * Set the default task stack size when creating tasks. * * The default is dependent on the device being used. Reducing the default stack * size yields greater memory savings. */ Task.defaultStackSize = 512; /* * Enables the idle task. * * Pick one: * - true (default) * Creates a task with priority of 0 which calls idle hook functions. This * option must be set to true to gain power savings provided by the Power * module. * - false * No idle task is created. This option consumes less memory as no * additional default task stack is needed. * To gain power savings by the Power module without having the idle task, * add Idle.run as the Task.allBlockedFunc. */ Task.enableIdleTask = true; //Task.enableIdleTask = false; //Task.allBlockedFunc = Idle.run; /* * If Task.enableIdleTask is set to true, this option sets the idle task's * stack size. * * Reducing the idle stack size yields greater memory savings. */ Task.idleTaskStackSize = 512; /* * Reduce the number of task priorities. * The default is 16. * Decreasing the number of task priorities yield memory savings. */ Task.numPriorities = 4; /* ================ Text configuration ================ */ var Text = xdc.useModule('xdc.runtime.Text'); /* * These strings are placed in the .const section. Setting this parameter to * false will save space in the .const section. Error, Assert and Log messages * will print raw ids and args instead of a formatted message. * * Pick one: * - true (default) * This option loads test string into the .const for easier debugging. * - false * This option reduces the .const footprint. */ //Text.isLoaded = true; Text.isLoaded = false; /* ================ Types configuration ================ */ var Types = xdc.useModule('xdc.runtime.Types'); /* * This module defines basic constants and types used throughout the * xdc.runtime package. */ /* ================ Application Specific Instances ================ */ var LoggingSetup = xdc.useModule('ti.uia.sysbios.LoggingSetup'); LoggingSetup.sysbiosLoggerSize = 1024; LoggingSetup.loadLogging = false;
当我运行代码并尝试启动执行分析工具时、不会发生任何情况。 我必须通过单击任务配置文件工具来启动该工具、然后选择执行图。 但它仍然只会生成空白/空白图。 我无法在工具中看到内核、但它确实显示在 Live Session 中。 希望您能帮我解决这个问题