This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280025C:DCSM -复位不再工作

Guru**** 2460850 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1125621/tms320f280025c-dcsm---reset-does-not-work-anymore

器件型号:TMS320F280025C

您好!

我有一个引导加载程序、当我不使用 DCSM 时、该引导加载程序相当不错(直接包含在项目中、如下 所示:https://www.ti.com/lit/an/spracp8a/spracp8a.pdf?ts=1656879106556)

我的 DCSM 设置如下所示:

引导加载程序链接器脚本如下所示:

-stack 0x380

MEMORY
{
   BEGIN           	: origin = 0x080000, length = 0x000002
   BOOT_RSVD		: origin = 0x00000002, length = 0x00000126
   RAMM0           	: origin = 0x00000128, length = 0x000002D8
   RAMM1            : origin = 0x00000400, length = 0x000003F8     /* on-chip RAM block M1 */
// RAMM1_RSVD       : origin = 0x000007F8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

/* RAMLS4           : origin = 0x0000A000, length = 0x00000800
   RAMLS5           : origin = 0x0000A800, length = 0x00000800
   RAMLS6           : origin = 0x0000B000, length = 0x00000800
   RAMLS7           : origin = 0x0000B800, length = 0x00000800*/

   /* Combining all the LS RAMs */
   RAMLS4567        : origin = 0x0000A000, length = 0x00002000
   RAMGS0           : origin = 0x0000C000, length = 0x000007F8
// RAMGS0_RSVD      : origin = 0x0000C7F8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */


   BOOTROM          : origin = 0x003F0000, length = 0x00008000
   BOOTROM_EXT      : origin = 0x003F8000, length = 0x00007FC0
   RESET            : origin = 0x003FFFC0, length = 0x00000002
   /* Flash sectors */
   /* BANK 0 */
   FLASH_BANK0_SEC0  : origin = 0x080002, length = 0x000FFE	/* on-chip Flash */
   FLASH_BANK0_SEC1  : origin = 0x081000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC2  : origin = 0x082000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC3  : origin = 0x083000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC4  : origin = 0x084000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC5  : origin = 0x085000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC6  : origin = 0x086000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC7  : origin = 0x087000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC8  : origin = 0x088000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC9  : origin = 0x089000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000	/* on-chip Flash */
   FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x000FF0	/* on-chip Flash */
// FLASH_BANK0_SEC15_RSVD     : origin = 0x08FFF0, length = 0x000010  /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

}

SECTIONS
{
   .reset           : > RESET, TYPE = DSECT /* not used, */
   codestart        : > BEGIN, ALIGN(4)

   .TI.ramfunc      : LOAD = (FLASH_BANK0_SEC0 | FLASH_BANK0_SEC1 | FLASH_BANK0_SEC2), /* This sector is loaded from flash to RAM */
	                  RUN = RAMLS4567,
	                  LOAD_START(RamfuncsLoadStart),
	                  LOAD_SIZE(RamfuncsLoadSize),
	                  LOAD_END(RamfuncsLoadEnd),
	                  RUN_START(RamfuncsRunStart),
	                  RUN_SIZE(RamfuncsRunSize),
	                  RUN_END(RamfuncsRunEnd),
	                  ALIGN(8)

   .text            : >> FLASH_BANK0_SEC0 | FLASH_BANK0_SEC1 | FLASH_BANK0_SEC2,   ALIGN(8) /* Programm is in flash */
   .cinit           : > FLASH_BANK0_SEC2,  ALIGN(4)
   .switch          : > FLASH_BANK0_SEC2,  ALIGN(4)
   .cio          	: > FLASH_BANK0_SEC2
   .pinit          	: > FLASH_BANK0_SEC2   ALIGN(4)
   .const           : > FLASH_BANK0_SEC2,  ALIGN(4)
   .init_array      : > FLASH_BANK0_SEC2,  ALIGN(4)

   .stack           : > RAMM1
   .bss             : > RAMM0
   .bss:output      : > RAMM0
   .bss:cio         : > RAMM0
   .data            : > RAMM0 /* Seems not to work, when using AES data --> leads to CRC error while updating, why? --> Needs separate RAM */
   .sysmem          : > RAMM0

   ramgs0 		    : > RAMGS0

    /*  Allocate IQ math areas: */
   IQmath           : > RAMM0
   IQmathTables     : > RAMM0

}

/*
//===========================================================================
// End of file.
//===========================================================================
*/

codestart.asm:

;//###########################################################################
;//
;// FILE:   flash_kernel_ex3_codestartbranch.asm
;//
;// TITLE: Branch for redirecting code execution after boot.
;//
;// For these examples, code_start is the first code that is executed after
;// exiting the boot ROM code.
;//
;// The codestart section in the linker cmd file is used to physically place
;// this code at the correct memory location. This section should be placed
;// at the location the BOOT ROM will re-direct the code to. For example,
;// for boot to FLASH this code will be located at 0x80000.
;//
;// In addition, the example f28002x projects are setup such that the codegen
;// entry point is also set to the codestart label. This is done by linker
;// option -e in the project build options. When the debugger loads the code,
;// it will automatically set the PC to the "entry point" address indicated by
;// the -e linker option. In this case the debugger is simply assigning the PC,
;// it is not the same as a full reset of the device.
;//
;// The compiler may warn that the entry point for the project is other then
;//  _c_init00. _c_init00 is the C environment setup and is run before
;// main() is entered. The codestart code will re-direct the execution
;// to _c_init00 and thus there is no worry and this warning can be ignored.
;//
;//###########################################################################
;// $Copyright:
;// Copyright (C) 2021 Texas Instruments Incorporated - http://www.ti.com/
;//
;// Redistribution and use in source and binary forms, with or without 
;// modification, are permitted provided that the following conditions 
;// are met:
;// 
;//   Redistributions of source code must retain the above copyright 
;//   notice, this list of conditions and the following disclaimer.
;// 
;//   Redistributions in binary form must reproduce the above copyright
;//   notice, this list of conditions and the following disclaimer in the 
;//   documentation and/or other materials provided with the   
;//   distribution.
;// 
;//   Neither the name of Texas Instruments Incorporated nor the names of
;//   its contributors may be used to endorse or promote products derived
;//   from this software without specific prior written permission.
;// 
;// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
;// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
;// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
;// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
;// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
;// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
;// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
;// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
;// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
;// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
;// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
;// $
;//###########################################################################

***********************************************************************

WD_DISABLE  .set  1    ;set to 1 to disable WD, else set to 0

    .ref _c_int00
    .ref main
    .global load_app_jump_addr
    .global code_start
    .global ExitBoot

***********************************************************************
* Function: codestart section
*
* Description: Branch to code starting point
***********************************************************************

    .sect "codestart"
    .retain

code_start:
    .if WD_DISABLE == 1
        LB wd_disable       ;Branch to watchdog disable code
    .else
        LB _c_int00         ;Branch to start of boot._asm in RTS library
        ;LCR main
    .endif

;end codestart section

***********************************************************************
* Function: wd_disable
*
* Description: Disables the watchdog timer
***********************************************************************
    .if WD_DISABLE == 1

    .text
load_app_jump_addr:
	LB ExitBoot

wd_disable:
    SETC OBJMODE        ;Set OBJMODE for 28x object code
    EALLOW              ;Enable EALLOW protected register access
    MOVZ DP, #7029h>>6  ;Set data page for WDCR register
    MOV @7029h, #0068h  ;Set WDDIS bit in WDCR to disable WD
    EDIS                ;Disable EALLOW protected register access
    LB _c_int00         ;Branch to start of boot._asm in RTS library
    ;LCR main

; Cleanup and exit.  At this point the EntryAddr
; is located in the ACC register
    ;BF ExitBoot, UNC

    .endif

;end wd_disable

;loadApplication:

	; Cleanup and exit.  At this point the EntryAddr
	; is located in the ACC register
    ;BF ExitBoot, UNC

;-----------------------------------------------
; ExitBoot
;-----------------------------------------------
;-----------------------------------------------
;This module cleans up after the boot loader
;
; 1) Make sure the stack is deallocated.
;    SP = 0x400 after exiting the boot
;    loader
; 2) Push 0 onto the stack so RPC will be
;    0 after using LRETR to jump to the
;    entry point
; 2) Load RPC with the entry point
; 3) Clear all XARn registers
; 4) Clear ACC, P and XT registers
; 5) LRETR - this will also clear the RPC
;    register since 0 was on the stack
;-----------------------------------------------

ExitBoot:

__stack:    .usect ".stack",0

;-----------------------------------------------
;   Insure that the stack is deallocated
;-----------------------------------------------

    MOV SP,#__stack

;-----------------------------------------------
; Clear the bottom of the stack.  This will endup
; in RPC when we are finished
;-----------------------------------------------

    MOV  *SP++,#0
    MOV  *SP++,#0

;-----------------------------------------------
; Load RPC with the entry point as determined
; by the boot mode.  This address will be returned
; in the ACC register.
;-----------------------------------------------

    PUSH ACC
    POP  RPC

;-----------------------------------------------
; Put registers back in their reset state.
;
; Clear all the XARn, ACC, XT, and P and DP
; registers
;
; NOTE: Leave the device in C28x operating mode
;       (OBJMODE = 1, AMODE = 0)
;-----------------------------------------------
    ZAPA
    MOVL  XT,ACC
    MOVZ  AR0,AL
    MOVZ  AR1,AL
    MOVZ  AR2,AL
    MOVZ  AR3,AL
    MOVZ  AR4,AL
    MOVZ  AR5,AL
    MOVZ  AR6,AL
    MOVZ  AR7,AL
    MOVW  DP, #0

;------------------------------------------------
;   Restore ST0 and ST1.  Note OBJMODE is
;   the only bit not restored to its reset state.
;   OBJMODE is left set for C28x object operating
;   mode.
;
;  ST0 = 0x0000     ST1 = 0x0A0B
;  15:10 OVC = 0    15:13      ARP = 0
;   9: 7  PM = 0       12       XF = 0
;      6   V = 0       11  M0M1MAP = 1
;      5   N = 0       10  reserved
;      4   Z = 0        9  OBJMODE = 1
;      3   C = 0        8    AMODE = 0
;      2  TC = 0        7 IDLESTAT = 0
;      1 OVM = 0        6   EALLOW = 0
;      0 SXM = 0        5     LOOP = 0
;                       4      SPA = 0
;                       3     VMAP = 1
;                       2    PAGE0 = 0
;                       1     DBGM = 1
;                       0     INTM = 1
;-----------------------------------------------

    MOV  *SP++,#0
    MOV  *SP++,#0x0A0B
    POP  ST1
    POP  ST0

;------------------------------------------------
;   Jump to the EntryAddr as defined by the
;   boot mode selected and continue execution
;-----------------------------------------------

    LRETR

;eof ----------

	.end


;//
;// End of file.
;//

那么、复位怎么会不再工作呢? DCSM 是否以某种方式移动了所有地址、并且无法跳转至开始?  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我现在可以实现、通过将所有闪存设置为"受此区域保护"而不 是"受此区域(EXEONLY)保护"、器件可以正确复位。

    现在、当我刷写器件时遇到另一个问题。 似乎、只有当 DCSM 处于活动状态时、情况才会发生。 引导加载程序可以在没有 CRC 错误的情况下将所有内容写入闪存、然后当它跳转到应用程序时、它会以某种方式进行砖型操作。 有什么想法、DCSM 可以与之相关吗? 我不会解锁任何区域等。当我写入闪存时、由于引导加载程序应该已经具有闪存访问权限、对吧? 我只使用 ti 的引导加载程序示例。

    编辑:

    似乎、 在闪存之前仍然需要调用 dcsm_unlockZone1CSM (&psCMDKey)、否则它将不起作用。 为什么?