主题中讨论的其他器件: C2000WARE
我已经修改了用于计算 TMS320F280025C 中64点 RFFT 的 RFFT 示例代码。 实现 RFFT 的完整主代码文件如下所示:
//############################################################################# // // FILE: main.c // // // //############################################################################# // $TI Release: F28002x Support Library v3.04.00.00 $ // $Release Date: Fri Feb 12 18:58:34 IST 2021 $ // $Copyright: // Copyright (C) 2021 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //############################################################################# // // Included Files // // Select the global Q value to use: #define GLOBAL_Q 17 #define FFT_SIZE 64 //long GlobalQ = GLOBAL_Q; // Used for legacy GEL & Graph Debug. #include "driverlib.h" #include "device.h" #include "board.h" #include "IQmathLib.h" #include <stdio.h> #include <file.h> #include "sci_io_driverlib.h" #include "fft.h" #include "fft_hamming_Q31.h" #include "math.h" // // Globals // uint16_t sData[32]; // Send data buffer for DMA transmission uint16_t rData[32]; // Receive data buffer for DMA reception //Defining FFT sections #pragma DATA_SECTION(ipcb, "FFTipcb"); int32_t ipcb[FFT_SIZE+2]; //Calculations buffer #pragma DATA_SECTION(ipcbsrc, "FFTipcbsrc"); int32_t ipcbsrc[FFT_SIZE]; //Sampled input signal //Defining real fft object for 64 point calculations RFFT32 rfft = RFFT32_64P_DEFAULTS; // Place buffers in GSRAM so that DMA can access these #pragma DATA_SECTION(sData, "ramgs0"); #pragma DATA_SECTION(rData, "ramgs0"); // // Function Prototypes void init_SPI_FIFO(void); // // Function Prototypes for Interrupt // extern __interrupt void controlISR(void); extern __interrupt void jemADCISR(void); extern __interrupt void cpuTimer0ISR(void); extern __interrupt void dmaCh5ISR(void); extern __interrupt void dmaCh6ISR(void); void initCPUTimers(void); void configCPUTimer(uint32_t, float, float); const long win[FFT_SIZE/2]=HAMMING64; void main(void) { volatile int status = 0; volatile FILE *fid; int i = 0; // float RadStep = 0.1963495408494f; float Rad = 0.0f; float temp1; int temp2; // // Initialize device clock and peripherals // Device_init(); // // Disable pin locks and enable internal pull-ups. // Device_initGPIO(); // // Initialize PIE and clear PIE registers. Disables CPU interrupts. // Interrupt_initModule(); // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // Interrupt_initVectorTable(); // // Interrupts that are used in this example are re-mapped to ISR functions // found within this file. // Interrupt_register(INT_TIMER0, &cpuTimer0ISR); Interrupt_register(INT_ADCA1, &controlISR); Interrupt_register(INT_ADCA2, &jemADCISR); // // Configuring interrupts for DMA transmit and receive channels Interrupt_register(INT_DMA_CH5, &dmaCh5ISR); Interrupt_register(INT_DMA_CH6, &dmaCh6ISR); // // Configure all peripherals and analog/digital GPIOs // Board_init(); //Initialize ADCs. Not generated by the sysconfig tool. ADC_init(); // //EPWM initialization code.Needs to be configured separately as current // tool version does not support this module // EPWM_init(); // Set up DMA for SPI use, initialize the SPI for FIFO mode initDMA(); //initSPI(); // Enable interrupts required for DMA send and receive // Interrupt_enable(INT_DMA_CH5); Interrupt_enable(INT_DMA_CH6); //Initialize Timer initCPUTimers(); // Configure CPU-Timer 0 to interrupt every 100000 u seconds: // configCPUTimer(CPUTIMER0_BASE, DEVICE_SYSCLK_FREQ, 100000); CPUTimer_enableInterrupt(CPUTIMER0_BASE); Interrupt_enable(INT_TIMER0); Interrupt_enable(INT_ADCA1); Interrupt_enable(INT_ADCA2); // // Enable Global Interrupt (INTM) and real time interrupt (DBGM) // EINT; ERTM; // Redirect STDOUT to SCI status = add_device("scia", _SSA, SCI_open, SCI_close, SCI_read, SCI_write, SCI_lseek, SCI_unlink, SCI_rename); fid = fopen("scia", "w"); freopen("scia:", "w", stdout); setvbuf(stdout, NULL, _IONBF, 0); //Prints welcome message on debug SCI printf("Skyelectric"); DEVICE_DELAY_US(10000); init_SPI_FIFO(); // Start the DMA channels // DMA_startChannel(DMA_CH6_BASE); DMA_startChannel(DMA_CH5_BASE); //------------------------------------ CPUTimer_startTimer(CPUTIMER0_BASE); //Temporary code for implementing FFT for (i=0;i<FFT_SIZE;i++) { ipcbsrc[i]=(long)(2147483648*sinf(Rad));//Q31 format Rad=Rad+0.09817; } printf("\r\nSample Input:\r\n"); for (i = 0; i < FFT_SIZE; i++) printf("%ld\r\n", ipcbsrc[i]); } RFFT32_brev(ipcbsrc, ipcb, FFT_SIZE); // real FFT bit reversing rfft.ipcbptr = ipcb; // FFT computation buffer rfft.magptr = ipcbsrc; // Magnitude output buffer rfft.winptr = (long *)win; // Window coefficient array rfft.init(&rfft); // Twiddle factor pointer initialization rfft.calc(&rfft); // Compute the FFT rfft.split(&rfft); // Post processing to get the correct spectrum rfft.mag(&rfft); // Q31 format (abs(ipcbsrc)/2^16).^2 printf("\r\nFFT Result:\r\n"); for (i = 0; i < FFT_SIZE; i++) { printf("%ld\r\n", ipcbsrc[i]); } for (;;) { DEVICE_DELAY_US(1000000); //one second delay } } void init_SPI_FIFO(void) { int i; for (i = 0; i < 32; i++) sData[i] = i; }
编译过程会引发以下大量错误:
项目的链接器设置如下所示:
下面显示了链接器命令文件、以检查 FFT 段是否已正确分配。
MEMORY
{
BEGIN : origin = 0x080000, length = 0x000002
BOOT_RSVD : origin = 0x00000002, length = 0x00000126
RAMM0 : origin = 0x00000128, length = 0x000002D8
RAMM1 : origin = 0x00000400, length = 0x000003F8 /* on-chip RAM block M1 */
// RAMM1_RSVD : origin = 0x000007F8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
/* RAMLS4 : origin = 0x0000A000, length = 0x00000800
RAMLS5 : origin = 0x0000A800, length = 0x00000800
RAMLS6 : origin = 0x0000B000, length = 0x00000800
RAMLS7 : origin = 0x0000B800, length = 0x00000800*/
/* Combining all the LS RAMs */
RAMLS4567 : origin = 0x0000A000, length = 0x00002000
RAMGS0 : origin = 0x0000C000, length = 0x000007F8
// RAMGS0_RSVD : origin = 0x0000C7F8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
// FLASHBANK1 : origin = 0x00080000, length = 0x0000FFF0
// FLASH_BANK1_RSVD : origin = 0x0008FFF0, length = 0x00000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
BOOTROM : origin = 0x003F0000, length = 0x00008000
BOOTROM_EXT : origin = 0x003F8000, length = 0x00007FC0
RESET : origin = 0x003FFFC0, length = 0x00000002
/*IQMath table already exists in the BOOTROM section*/
//IQTABLES : origin = 0x3F1402, length = 0x0166D
/* Flash sectors */
/* BANK 0 */
FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x000FFE /* on-chip Flash */
FLASH_BANK0_SEC1 : origin = 0x081000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC3_9 : origin = 0x083000, length = 0x007000 /* on-chip Flash */
FLASH_BANK0_SEC10_11 : origin = 0x08A000, length = 0x002000 /* on-chip Flash */
FLASH_BANK0_SEC12_15 : origin = 0x08C000, length = 0x003FF0 /* on-chip Flash */
// FLASH_BANK0_SEC15_RSVD : origin = 0x08FFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
}
SECTIONS
{
codestart : > BEGIN, ALIGN(8)
.text : >> FLASH_BANK0_SEC2 | FLASH_BANK0_SEC3_9 , ALIGN(8)//executable code >> operator splits code
.cinit : > FLASH_BANK0_SEC1, ALIGN(8)//table that initializes global variables
.switch : > FLASH_BANK0_SEC1, ALIGN(8)
.reset : > RESET, TYPE = DSECT /* not used, Dummy Section*/
.stack : > RAMM1
.init_array : > FLASH_BANK0_SEC1, ALIGN(8)
.bss : > RAMLS4567 //uninitialized global variables
.bss:output : > RAMLS4567
.bss:cio : > RAMGS0
.const : > FLASH_BANK0_SEC10_11, ALIGN(8)
.data : > RAMLS4567 //initialized data
.sysmem : > RAMLS4567
ramgs0 : > RAMGS0
/* Allocate IQ math areas: */
IQmath : > FLASH_BANK0_SEC1, PAGE = 0, ALIGN(4) /* Math Code */
//IQmathTables : > FLASH_BANK0_SEC2, PAGE = 0, ALIGN(4)/*This was working*/
IQmathTables : > FLASH_BANK0_SEC1, PAGE = 0, ALIGN(4)/*Moved to sector 1 to run from RAM.Need verification*/
/* Allocating FFT areas: */
FFTipcb : >> RAMGS0, ALIGN(256) //64 points FFT
FFTipcbsrc : >> RAMLS4567
FFTtf : > FLASH_BANK0_SEC12_15
.TI.ramfunc : LOAD = FLASH_BANK0_SEC1, //Flash bank0 sector 1 contaings time critical functions required to run from RAM
RUN = RAMGS0,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
请注意、我仅在一个月前就开始使用 TI 控制器、我不熟悉链接的命令文件、因此请验证是否正确分配了所有段。 如果能够修改这些分配 以获得更好的处理时间和更高效的内存使用、我将不胜感激。 同时、我将查看 C2000Ware 目录中的"定点 DSP 软件库"文档、以便在我结束时进行故障排除 我参考了为 f2838x 控制器编写的"FixedPoint_RFFT"项目。