请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:ADS8902B 我想测量振幅调制4V p-p 100kHz 正弦波的振幅、分辨率为18-20位。 我可以了
将其解调为2V p-p 整流正弦波、低通滤波器、放大并以200ksps 采样、或
2.在峰值、200ksps 时同步采样并进行数字解调
哪一项是更低的噪声? 2) 2)更简单、不会出现1/f 噪声、但总噪声是否会更低?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.