请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TI-API 积压报价 API 错误代码是什么意思?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
情况 | 错误详细信息 | 补救步骤 |
CustomerEndCustomerName 和 SupplierEndCustomerIdentifier 缺失 | { "errors": [ { "Code": "TI-VAL-0001", "Type": "ERROR", "Message": "Provide CustomerEndCustomerName or SupplierEndCustomerIdentifier and resubmit the request." } ] } |
提供 CustomerEndCustomerName 或 SupplierEndCustomerIdentifier 并重新提交请求。 |
客户报价商品数量缺失 | { "errors": [ { "Code": "TI-VAL-0003", "Type": "ERROR", "Message": "Provide a valid CustomerQuoteItemQuantity number for each line item and resubmit the request." } ] } |
为每个行项目提供有效的 CustomerQuoteItemQuantity 号码并重新提交请求。 |
客户标识符和供应商标识符缺失 | { "errors": [ { "Code": "TI-VAL-0005", "Type": "ERROR", "Message": "Provide CustomerSoldToIdentifier or SupplierSoldToIdentifer and resubmit the request." } ] } |
提供 CustomerSoldToIdentifier 或 SupplierSoldToIdentfer 并重新提交请求。 |
客户报价标识符无效 | { "errors": [ { "Code": "TI-VAL-0006", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerQuoteIdentifier up to 35 characters and resubmit the request." } ] } |
提供有效的客户报价单标识符(最多35个字符)、然后重新提交请求。 |
CustomerQuoteReason 无效 | { "errors": [ { "Code": "TI-VAL-0007", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid 2-character CustomerQuoteReason and resubmit the request." } ] } |
提供有效的2个字符的 CustomerQuoteReason 并重新提交请求。 |
SupplierSoldToIdentifier 和 CustomerSoldToIdentifier 缺失或无效 | { "errors": [ { "Code": "TI-VAL-0008", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid SupplierSoldToIdentifier (1-10 characters) or CustomerSoldToIdentifier (1-20 characters) and resubmit the request." } ] } |
提供有效的 SupplierSoldToIdentifier (1-10个字符)或 CustomerSoldToIdentifier (1-20个字符),然后重新提交请求。 |
CustomerContactName 无效 | { "errors": [ { "Code": "TI-VAL-0009", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerContactName up to 40 characters and resubmit the request." } ] } |
提供有效的 CustomerContactName (客户联系人姓名),最多40个字符,然后重新提交请求。 |
CustomerContactEmailAddress 无效 | { "errors": [ { "Code": "TI-VAL-0010", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerContactEmailAddress up to 75 characters and resubmit the request." } ] } |
提供有效的 CustomerContactEmailAddress (客户联系人电子邮件地址),最多75个字符,然后重新提交请求。 |
CustomerContactPhoneNumber 无效 | { "errors": [ { "Code": "TI-VAL-0011", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerContactPhoneNumber up to 30 characters and resubmit the request." } ] } |
提供有效的 CustomerContactPhoneNumber (最多30个字符),然后重新提交请求。 |
CustomerEndIdentifier 无效 | { "errors": [ { "Code": "TI-VAL-0012", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerEndCustomerIdentifier up to 20 characters and resubmit the request." } ] } |
提供有效的 CustomerEndCustomerIdentifier (最多20个字符),然后重新提交请求。 |
CustomerEndCustomerName 和 SupplierEndCustomerIdentifier 缺失或无效 | { "errors": [ { "Code": "TI-VAL-0013", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerEndCustomerName (1-52 characters) or SupplierEndCustomerIdentifier (1-10 characters) and resubmit the request." } ] } |
提供有效的 CustomerEndCustomerName (1-52个字符)或 SupplierEndCustomerIdentifier (1-10个字符),然后重新提交请求。 |
CustomerEndCustomerCity 无效 | { "errors": [ { "Code": "TI-VAL-0014", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerEndCustomerCity up to 40 characters and resubmit the request." } ] } |
提供有效的 CustomerEndCustomerCity (最多40个字符),然后重新提交请求。 |
CustomerEndCustomerCountrry 无效 | { "errors": [ { "Code": "TI-VAL-0015", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid 2-character CustomerEndCustomerCountry and resubmit the request." } ] } |
提供有效的2个字符的 CustomerEndCustomerCountrry 并重新提交请求。 |
CustomerEndCustomerPostalCode 无效 | { "errors": [ { "Code": "TI-VAL-0016", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerEndCustomerPostalCode up to 10 characters and resubmit the request." } ] } |
提供有效的 CustomerEndCustomerPostalCode (最多10个字符),然后重新提交请求。 |
CustomerQuoteLineItemNumber 无效 | { "errors": [ { "Code": "TI-VAL-0017", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerQuoteLineItemNumber up to 10 characters and resubmit the request." } ] } |
提供有效的客户报价行项目号(最多10个字符)、然后重新提交请求。 |
客户能力供应商货币无效 | { "errors": [ { "Code": "TI-VAL-0018", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerCompetingSupplierCurrency up to 5 characters and resubmit the request." } ] } |
提供最多5个字符的有效客户能力 SupplierCurrency 并重新提交请求。 |
客户能力 SupplierUnitPrice 无效 | { "errors": [ { "Code": "TI-VAL-0019", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerCompetingSupplierUnitPrice number value up to 19 digits and resubmit the request." } ] } |
提供有效的 CustomerCompetingSupplierUnitPrice 编号值(最多19位),然后重新提交请求。 |
CustomerCompetingSupplierMaterial 无效 | { "errors": [ { "Code": "TI-VAL-0020", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerCompetingSupplierMaterial up to 40 characters and resubmit the request." } ] } |
提供有效的客户能力供应商材料(最多40个字符)并重新提交请求 |
CustomerCompetingSupplierName 无效 | { "errors": [ { "Code": "TI-VAL-0021", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerCompetingSupplierName up to 40 characters and resubmit the request." } ] } |
提供有效的 CustomerCompetingSupplierName (客户能力供应商名称),最多40个字符,然后重新提交请求。 |
CustomerTargetUnitPrice 无效 | { "errors": [ { "Code": "TI-VAL-0022", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerTargetUnitPrice number value up to 19 digits and resubmit the request." } ] } |
提供有效的 CustomerTargetUnitPrice 编号值(最多19位),然后重新提交请求。 |
CustomerQuoteItemQuantity 无效 | { "errors": [ { "Code": "TI-VAL-0023", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerQuoteItemQuantity number value up to 13 digits and resubmit the request." } ] } |
提供有效的 CustomerQuoteItemQuantity Number 值(最多13位)、然后重新提交请求。 |
CustomerProductIdentifier 无效 | { "errors": [ { "Code": "TI-VAL-0024", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerProductIdentifier up to 40 characters and resubmit the request." } ] } |
提供有效的 CustomerProductIdentifier (客户产品标识符),最多40个字符,然后重新提交请求。 |
SupplierProductIdentifier 无效 | { "errors": [ { "Code": "TI-VAL-0025", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid SupplierProductIdentifier up to 40 characters and resubmit the request." } ] } |
提供有效的 SupplierProductIdentifier (供应商产品标识符)、最多40个字符、然后重新提交请求。 |
客户中介客户标识符无效 | { "errors": [ { "Code": "TI-VAL-0026", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerIntermediateCustomerIdentifier up to 20 characters and resubmit the request." } ] } |
提供有效的 CustomerIntermediaCustomerIdentifier (最多20个字符),然后重新提交请求。 |
客户中介 CustomerName 无效 | { "errors": [ { "Code": "TI-VAL-0027", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerIntermediateCustomerName up to 52 characters and resubmit the request." } ] } |
提供有效的客户中介 CustomerName (客户名称),最多52个字符,然后重新提交请求。 |
Supplier中介 客户标识符无效 | { "errors": [ { "Code": "TI-VAL-0028", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid SupplierIntermediateCustomerIdentifier up to 10 characters and resubmit the request." } ] } |
提供有效的 Supplier中介 客户标识符(最多10个字符)并重新提交请求。 |
CustomerIntermediateCustomerCity 无效 | { "errors": [ { "Code": "TI-VAL-0029", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerIntermediateCustomerCity up to 40 characters and resubmit the request." } ] } |
提供有效的 CustomerIntermediaCustomerCity (最多40个字符),然后重新提交请求。 |
客户中介客户计数无效 | { "errors": [ { "Code": "TI-VAL-0030", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid 2-character CustomerIntermediateCustomerCountry and resubmit the request." } ] } |
提供有效的2个字符的 CustomerIntermediaCustomerCountrry 并重新提交请求。 |
客户中介客户邮政编码无效 | { "errors": [ { "Code": "TI-VAL-0031", "Type": "ERROR", "Message": "Line Item {n}: Provide a valid CustomerIntermediateCustomerPostalCode up to 10 characters and resubmit the request." } ] } |
提供有效的 CustomerIntermediaCustomerPostalCode (最多10个字符),然后重新提交请求。 |
报价类型无效 | { "errors": [ { "Code": "TI-VAL-0032", "Type": "ERROR", "Message": "Provide a valid QuoteType or remove the field and resubmit the request." } ] } |
提供有效的报价类型或删除该字段并重新提交申请。 |
发生系统错误 | { "errors": [ { "Code": "TI-VAL-50000", "Type": "ERROR", "Message": "Please contact TI API Support (https://api-portal.ti.com/support)." } ] } |
请联系 TI API 支持(api-portal.ti.com/support)。 |
CustomerQuoteIdentifieris invalid (客户报价识别器无效) | { "errors": [ { "Code": "TI-TXT-001", "Type": "ERROR", "Message": "Validate your quote ID and resubmit the request." } ] } |
提供有效的客户报价单标识符(最多35个字符)、然后重新提交请求。 |