This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN74AHC574:引脚9和引脚11均连接到25MHz CLK

Guru**** 2511985 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/1002399/sn74ahc574-both-of-pin9-and-pin11-connect-to-25mhz-clk

器件型号:SN74AHC574

大家好、

您能否帮助确认我们是否可以同时将25MHz 时钟连接到引脚9和 P11?

罗伊