This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN74LXC2T45-Q1:能不能在125 MHz 时支持 IO 电平0.69V 转换为1V?

Guru**** 2507315 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/1238652/sn74lxc2t45-q1-can-support-for-io-level-0-69v-translate-to-1v-at-125mhz

器件型号:SN74LXC2T45-Q1

您好!  

该转换器可以在125 MHz 的频率下将 IO 从0.69V 转换为1V?

而 VCCA 电源为1.1V 至5V、但阈值高电压为0.44V 至0.88V。  

您能评论一下吗?