Other Parts Discussed in Thread: TXB0304, TXB0104
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TXB0304 主题中讨论的其他器件: TXB0104
大家好、
TXB0304和 TXB0104之间有何差异?
尼森
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TXB0304输出具有较低阻抗(1 kΩ 而非4 kΩ)。 这意味着 TXB0304要求其他器件具有更高的驱动强度、但它支持更高的速度。 仅 TXB0104支持5V。