This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DRV8301:关于引导电容器

Guru**** 651100 points
Other Parts Discussed in Thread: DRV8301, DRV8300
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1089267/drv8301-about-bootstrap-capacitor

部件号:DRV8301
主题中讨论的其他部件: DRV8300

您好,

我想询问有关使用Drv8301进行引导电容器选择的问题。

在Drv8301 EVM套件板上,电路板上使用0.1uF自举电容器。

我不知道当我们增加PWM频率时,我们是否应该更改自举电容器值。

例如,如果我在80kHz的Drv8301中使用PWM,我们应该使用小于0.1uF的自举电容器值?

此致,

Hiroyasu Matsubara