This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS62135:我们能否在设计中使用3.1A ITEMP/3.7A Isat 电感器?

Guru**** 2511415 points
Other Parts Discussed in Thread: TPS62135

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/944522/tps62135-can-we-use-a-3-1a-itemp-3-7a-isat-inductor-for-our-design

器件型号:TPS62135

大家好、

我有一位客户使用2个 TPS62135、需要为他们的应用找到尺寸最佳的电感器、因为空间是一个主要限制因素。

其设计要求为:

输入:6-9V

输出:3.6V (第一个稳压器)和5.5V (第二个稳压器)

最大输出电流:2A (最大值)

温度:预计为60C

他们能否可靠地使用数据表第14页的表3 (电感器列表)中推荐的最后一个电感器(1277AS-H-1R0M (DFE322512C)?

问题是电感器的电流限制过低。  

谢谢、

赖凯文