请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS62745 主题中讨论的其他器件:TPS62125、 TPS62175
尊敬的专家:
我的客户正在为4节锂锰电池电源应用选择降压转换器、他们的需求如下:
- 15V 输入电压、3.3-5V 输出电压、>=300mA
- 低 Iq (TPS62125对于它们来说太大)
- 高效率
我们是否有类似 TPS62745的超低 IQ 器件? 感谢您的支持。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.