请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS546C23 我的带 TPS546C23的单相应用不使用 PMBus、如何连接以下信号?
- ADDR0
- 地址1
- PMB_DATA
- PMB_CLK
- SMB_ALRT
可能性:
- 未连接
- 100千欧接地
- 100k Ω 至 BP3 (片上稳压器)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.