请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ76930 大家好、
BQ76930规范中描述的 ADC 测量范围值、电池电压范围为2至5V。 当实际电池的电压值小于2V (例如1.8V)时、BQ76930将向 MCU 上载哪种电压值?
请帮助回答此问题吗?
此致、谢谢!
雪利
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.