您好!
我在项目中使用 TPS40170。 这是我的要求
输入 VDC:48 VDC、±10%
输出 VDC:35 VDC @ 6A
问题:
当我以48VDC (空载)为器件上电时、器件会损坏。 所有电压电平均高于42VDC。
如果输入电压低于或等于42、则工作正常。
但我的要求是48VDC@±10%。
请您能帮我解决这个问题吗?
谢谢
Ashok
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.