请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS7A94 按照数据表图8-27第49页的"典型应用电路"设置低压降稳压器、并将引脚7的电阻设置为26.7k 欧姆、这应将输出电压设置为4.0V、 我得到的是4.7V 输出电压、并且将电阻器(NR/SS)更改为24.3K 对输出电压没有影响(停留在4.7V)、请见我的原理图下方、我按照数据表进行了布局、并且所有连接均按照原理图进行
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
按照数据表图8-27第49页的"典型应用电路"设置低压降稳压器、并将引脚7的电阻设置为26.7k 欧姆、这应将输出电压设置为4.0V、 我得到的是4.7V 输出电压、并且将电阻器(NR/SS)更改为24.3K 对输出电压没有影响(停留在4.7V)、请见我的原理图下方、我按照数据表进行了布局、并且所有连接均按照原理图进行