请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TPS61376、 TLV61048请推荐我一个直流/直流升压充电器 IC
- 输入:5V/2A
- 输出电压(电池):带 NTC 时为8.4V
- 恒流/恒压
- LED 指示灯:充电、充电完成、NTC (温度输入)
- 电池 NTC 输入
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.