请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5034 大家好、
数据表显示了当 UVLO 引脚= 1.3V 时76%的最大占空比、
但波形仅显示 68%。 请帮助检查 LM5034的这个问题。 谢谢。


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.