请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LMR38020 您好,
我将 LMR38020用于具有3个输出的直流/直流 Flybuck 转换器200mA、其中两个不是隔离式(3.3V/1.5A 和12V/PWM)、其中一个是隔离式(100mA)。 但满载时3.3V 输出电压纹波非常大、我该如何解决?
感谢你能抽出时间。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.