This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ24171:TS 引脚设置

Guru**** 2511415 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1218409/bq24171-ts-pin-setting

器件型号:BQ24171

大家好、TI 电源团队

我不想为高于45°C 的电池充电。

1.是否可以通过在校准工具的 R-HOT 中输入一个45°C 电阻值来设置它?
示例) 103AT:45°C = 4.91K/ 60°C = 3.02K

2.如果将 R-hot 设置为45°C 电阻值(4.91K)、那么 T2、T3和 T4漂移多少?

谢谢!