请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM285-1.2
工具与软件:

LM285DR-1-2的数据表中提供了两个电压容差值。 需要了解 LM285DR-1-2具有1%还是2%的初始电压容差。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
器件型号:LM285-1.2
工具与软件:

LM285DR-1-2的数据表中提供了两个电压容差值。 需要了解 LM285DR-1-2具有1%还是2%的初始电压容差。
尊敬的 Yuvhashree:
LM285-1.2提供1%的 电压容差。 
谢谢!
约书亚